ChangeFit™ Labs

The Labs

Each ChangeFit™ Lab is based on evidence of adaptability and resilience, and is used effectively with any and all size groups. Portions of the Labs have shown success in various branches of the military and with returning veterans adaptability and re-integration.

The Labs are boot camps in change readiness. They drill down in the underlying traits that will prepare people for the future - no matter what! They are fun, remarkably cost-effective and ... they work.

  1. The three labs can be taken alone.
  2. We contract mostly with small businesses with up to 500 employees or single departments of larger companies.
  3. Most Labs are conducted in small groups but individuals can follow the online course.
  4. Private executive coaching is included and is currently booking into 2018.



Begin by taking an intro to the CFAT Change Fit™ Assessment: