Five Things You Should Never Do with Other People

1. Anything for anyone over the age of 18 that they can and should be doing for themselves. This behavior weakens the recipient and usually causes resentment in the caregiver. Resentment is powerfully disabling an leads to other bad habits you don’t need. If you are rescuing anyone over 18, you are not helping them. Rather, you are meeting your own unmet needs and it is time to meet those from other sources.

2. Fix them. Similar to #1, this drainer tries to change what can’t be controlled. The motivation is typically a kindly one, a genuine effort to make sure that others are safe. You believe that you have the answer to other people’s problems and if only they would listen to you, their lives would be better. Unfortunately, you create only resentment in both them, and in you–after all you have done for them! People don’t want to be told what to do. Your greatest gift would be to accept them the way they are. It’s not your path. Let them live their lives. If they ask for help then step in, but otherwise, read #1 again.

3. React to their bad behavior. Take nothing personally, it’s never about you. Don Miguel Ruiz’s analogy of our individual theaters and personal movies is helpful. Each of us is sitting in front of our own films, in our own theaters. We are the star of our own movie, with our chosen cast of characters. Some have leading roles, some supporting roles, and many are extras. Issues develop when we demand to be the star of someone else’s movie, or we insist on a larger role than their script calls for. People run their own script and their own movie. Other people’s behaviors are not directed at you. Stop being injured over the injustices that people do to you, because they are not doing it to you. They are just doing it. When you can get this, you free up more energy you need to prevent the injustices from being done in the first place. It is a more effective use of energy to instruct others how to behave in your presence, and what minimum standards you expect.

4. Compare yourself to them. Comparing yourself to others, either in a positive or negative way, is doomed to failure. Don’t compare. Instead, measure your growth as a rough percentage of change using your own baseline. Ask yourself: “Am I a percentage better at this than I was last year? Six months ago?” Perhaps 20% better? If so, your goals are being met. The only comparison to do is with your former self, and the only projections will be to your future self. Others will always have more or less than you have, because they are walking on a different path. Is the path better than yours? No, it’s just different. You label it as better. Comparing yourself is a low self-image activity, one that you no longer need. It is energy not well spent, because it doesn’t change where you are and move you toward where you want to be.

5. Get Impatient. Not for them. For you. Sure, it can make you unbearable to be around. But you are just wasting energy getting mad at situations and other people, wishing they would do things differently, wishing they would get out of your way, wanting them to be different than they are. Hitting the elevator button repeatedly and yelling “Hurry up!!” won’t bring the elevator any faster.

Impatience is one factor in Type A Behavior. The hostility that goes along with impatience can, and will, kill you. Choose where you spend energy. Discipline yourself to ‘let it go.’ When you are tempted to intervene in others’ lives in ways such as giving advice or hurrying people up, just relax, take a big breath, and let it go. Repeat this sentence whenever you feel frustration with the way things are: “Grant me the serenity to accept the things I cannot change, the courage to change the things I can, and the wisdom to know the difference.”  Lack of patience can result from a belief that the world should center around you and not interfere with your comings and goings. People should do things your way because you know better. If everyone did what they were supposed to do, the world would be a better place and you would be much happier. If you can see that this thinking isn’t paying off, congratulations, you’re half way there!

What do you think?